Program stuck in __aeabi_uldivmod in KEA64

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Program stuck in __aeabi_uldivmod in KEA64

1,877 Views
mohmdshibin
Contributor I

Hi,

I am using KEA64 evaluation kit and JLink debugger in CodeWarrior. But the program is stuck in __aeabi_uldivmod. I have no idea why it is happening. Please share your thoughts on the issue.

Thank you!

0 Kudos
Reply
2 Replies

1,769 Views
mohmdshibin
Contributor I

The software stuck in function __init_hardware() in startup code.

0 Kudos
Reply

1,769 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Mohammed,

    Please tell me your KEA64 full name, then check it with your project, do you select the correct chip with your project?

   I need to make sure your project and the KEA64 chip is match, as you know the KEA64 have the S9KEAZN64xxx and S9KEAZ64xxx, these two chip have a lot of register difference. Please check this point at first.

   Besides, you also can create a new empty project for your KEA64 in the CW, can you also meet this stuck problem?


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply