Product Selection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Product Selection

1,698件の閲覧回数
psh1
Contributor I

Recently, we are trying to develop a DC meter (Class 0.5) by increasing use of DC.

So I want to use the MKM33Z or MCF51EM Series.


But if you have another MCU that is suitable for DC meter, I would like to recommend it.

I will wait for your reply.

Best regard.

0 件の賞賛
返信
2 返答(返信)

1,629件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi,

It is depend on what function do you need. If your design is not very complex, I think KM1x is also a good choice.

https://www.nxp.com/products/processors-and-microcontrollers/arm-based-processors-and-mcus/kinetis-c...

Regards,

Jing

0 件の賞賛
返信

1,629件の閲覧回数
psh1
Contributor I

Hello, Jing.

Thank you for good information.

Thank you for helping me.

Best regard.

2018-06-01 12:38 GMT+09:00 jingpan <[email protected]>:

NXP Community

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: Product Selection

reply from Jing Pan

<https://community.nxp.com/people/jingpan?et=watches.email.thread> in *Kinetis

Microcontrollers* - View the full discussion

<https://community.nxp.com/message/1020309?commentID=1020309&et=watches.email.thread#comment-1020309>

0 件の賞賛
返信