Processor Expert PWM settings in complementary mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Processor Expert PWM settings in complementary mode

1,366件の閲覧回数
capvdesign
Contributor II

We need to use the PWM EP complementarily component.

In addition to put each pin independien way into a known state.

Serious frequency 40Khz

The micro MKE02Z64VQH4

Pines PTC0 - PTC1 and PTC2-PTC3.

Disable the pwm and access directly to the pins to change the status.

Thanks.

Carlos Pichardo

ラベル(1)
0 件の賞賛
返信
1 返信

1,224件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi CARLOS PICHARDO

After checking the requirements of your project we believe it is not possible to make use of the pins as GPIOs when the FTM2 module is active, this is because the peripheral modules have priority over the I/O, so when a peripheral is enabled, the associated I/O functions are disabled. If you want to control the pins as GPIOs you will have to disable the FTM2 module causing all of it channels to be disabled too.

Hope this information helps!

Best Regards

Jorge Alcala

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信