Problems with Mouse example code on TWR-K60D100M based tower kit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problems with Mouse example code on TWR-K60D100M based tower kit

1,695件の閲覧回数
MWMinor
Contributor V

Hi

I am using a TWR-K60D100M board with a tower kit to try and develop some knowledge of the USB as a CDC device. I've built and downloaded the hid_mouse project for this board and it seemed to load OK, but when I tried connecting a USB cable to the USB mini-connector on the TWR-SER board I get no activity detected.

I'm using CWV10.6 and MQX4.1.

Can anyone help with this please...?

Thanks

Ken

0 件の賞賛
返信
2 返答(返信)

1,537件の閲覧回数
adriancano
NXP Employee
NXP Employee

Hi,

To run this application you need to set some jumpers in the TWR-SER board to enable the Device functionality, check the document MQX_Getting_Started.pdf in the MQX installation folder (Freescale_MQX_4_1\doc) in the page 53, you can find there the jumper setting for different functionalities.

  For the TWR-K60D100M you can see this (there is an error in the document with the name of the jumpers, here you can see the real order):

USB device twr ser.png

I hope this information can help you.


Regards,

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. It would be nice!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,537件の閲覧回数
MWMinor
Contributor V

Hi

Thanks for the reply. I've checked those link positions and they are correct.

When I plug the PC into this port on the TWR-SER board it doesn't enumerate (and doesn't make the usual "beep" ) and doesn't recognise anything is plugged in.

Can you help please...?

Thanks

0 件の賞賛
返信