Problems using PIT to trigger a DMA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problems using PIT to trigger a DMA

3,221 Views
arnoldbischof
Contributor III

I have implemented a driver which periodically converts all AD channels and transfers the results within DMA to RAM. In my first version I used the PDB to trigger the DMA which starts the conversion sequence. This version worked fine. In my second version, I want to use a PIT (with same number as the DMA channel) which triggers the DMA. This version is not able to run because I get immediately after enabling the PIT a DMA SBE error (Source Bus Error) on the channel which is used by the conversion sequence.

Is there anybody who can help me with this issue?

Labels (1)
Tags (5)
0 Kudos
Reply
4 Replies

2,550 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Arnold,

From your description, it just use PIT instead of PDB module as hardware trigger source of ADC conversion. There without any modification with DMA trigger with ADC conversion finish.

If customer just set PIT to period trigger DMA? It need to use ADC trigger DMA when ADC conversion finished.

And customer need to check SIM_SOPT7 to select correct ADC hardware trigger source.


Wish it help.

best regards,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,550 Views
arnoldbischof
Contributor III

Hello Ma Hui

I think you do misunderstand my problem.

Please read the description of my ADC DMA driver in following Link Re: scanning all ADC channels within DMA

The only difference, as described in the new Post 'Problems using PIT to trigger a DMA' is that I use the PIT instead of the PDB to trigger the DMA.

0 Kudos
Reply

2,550 Views
mjbcswitzerland
Specialist V

Arnold

I haven't used a PIT for DMA triggering but have noticed that there is an errata concerning the DMAMUX and PIT (eg. Errate ID 4588).

Have you checked the errate to the mask used in your chip? Could something like this be a cause of difficulty?

Regards

Mark

2,550 Views
arnoldbischof
Contributor III

Hi Mark

It seems this is the reason for my problem. So I try to use an other timer e.g. an FTM

Thanks

Arnold

0 Kudos
Reply