Problem with release version for kea 128

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem with release version for kea 128

1,142 Views
EmanueleP
Contributor II
Hi,
I have a problem flashing my firmware in the kea128.
I'm using s32 studio as my development environment. When I switch to the release build,
I get an elf file that I use as the "C/C++ Application:" parameter in
"flash configuration". (I've never had any problems with debug build)
 

When the flash procedure is finished I try to power my device and I discover that the
fw has not been loaded correctly (the development environment does not provide any
type of error). Can someone help me?

Thank you!
 

 

0 Kudos
Reply
1 Reply

1,120 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Please refer to the discussion here, hope it helps: how to use the build target--Release for S32DS for ARM project


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply