Problem with USB enumeration on K60 board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem with USB enumeration on K60 board

1,753件の閲覧回数
MWMinor
Contributor V

Hi there

I have been having some problems with getting the USB port on my custom K60-based board, enumerating over VSB. Using the example virtual-com port as a starting point, I connected the USB to a laptop running Windows 7 and the laptop identifies the "device" as a HID - not a COM port. I have tried a different laptop, but the response is the same. I compiled the example and loaded it onto a TWRK60D100 board. The results were the same again.

Has anyone else had similar problems....??

Thanks

Ken

2 返答(返信)

1,528件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Ken:

Can you point me to the specific demo you are using?

If this demo application belongs to the USB stack please provide a couple details.

- USB stack version.

- IDE.

- Path to the specific demo.

:smileyinfo: Remember always posting to specialized community spaces, such as Kinetis Microcontrollers. Otherwise your questions have very low visibility to the community audience.

Regards!

Jorge Gonzalez

0 件の賞賛
返信

1,528件の閲覧回数
MWMinor
Contributor V

Hello Jorge

Many thanks for getting back to me and apologies for the delay in responding to your answer....

I found the root cause of the problem I was experiencing being a file that I had somehow included in the build - usb_init.c - which included the setup for a USB_HID. Once this was removed, the problem went away.

I appreciate your responding though.....

Regards

Ken