Problem updating bootloader for FRDM-KE06Z

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem updating bootloader for FRDM-KE06Z

Jump to solution
3,330 Views
seanbeatty
Contributor III

I purchased a new FRDM-KE06Z board and attempted to update the bootloader. Before updating, SDA_INFO.html showed:

     MicroBoot Kernal Version: 1.05

     Bootloader Version is: 1.10

     Application Version is: 1.14

The Led blinked at a 1 Hz rate.

Then I tried to update the bootloader according to the P&E instructions - put the Freedom board into bootloader mode by holding down the reset button and powering up, verify the volume is labeled "BOOTLOADER", and dragging the BOOTUPDATEAPP_Pemicro_v111.SDA file to the drive. Then unplug the USB cable, plug it back in, and wait while it programs ....

After a few seconds, the LED starts flashing rapidly 7 or 8 times, then off for a second or two, then flashing rapidly ... repeating this pattern. SDA_INFO now shows:

Board Name is: FRDM-KE06Z
MicroBoot Kernel Version is: 1.05
Bootloader Version is: 1.10
Application Version is: 0.00
DUID is: 30133938-8F0281E2-3762D80E-B76DE678
EUID is: 2691A239-2068876C-1861FA19-957668D6
TUID is: 74823938-8063C6C9-3736F906-92389865
TOA is: 86B6E505-CA5272BA-230F3A9F-D5E34335
TOA2 is: 86B6E505-79398CC7-CE85F4A6-80964A1D
SUID is: 86B6E505-4D5A8397-37239806-8003EC65

It appears that the reprogramming failed. I can no longer power up the board normally into the FRDM-KE06 volume like previously - it always goes into the BOOTLOADER volume.

I tried this on three different boards. For the last attempt, I also disabled the virus scanner and firewall, and performed the copy using the Command Prompt (DOS) window, as suggested by some. I got the same results.

What happened? How do I recover?

Thanks for your help!

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
2,856 Views
seanbeatty
Contributor III

I ended up programming everything on an old Windows XP machine. That worked!

Apparently, my issues were due to Windows 10.

Issue closed from my perspective.

View solution in original post

0 Kudos
Reply
3 Replies
2,857 Views
seanbeatty
Contributor III

I ended up programming everything on an old Windows XP machine. That worked!

Apparently, my issues were due to Windows 10.

Issue closed from my perspective.

0 Kudos
Reply
2,856 Views
BlackNight
NXP Employee
NXP Employee

Hi Sean,

have you extracted the file first onto your disk (you cannot drag&drop the file from the zip file).

you might try to copy it with the DOS prompt too.

The board comes up in bootloader mode because not application is loaded:

Application Version is: 0.00

Otherwise: Illustrated Step-by-Step Instructions: Updating the Freescale Freedom Board Firmware | MCU on Eclips...

I hope this helps,

Erich

0 Kudos
Reply
2,856 Views
seanbeatty
Contributor III

Erich –

Yes, I unzipped the file – it has an “.sda” extension. I did try copying it with the DOS prompt. No results.

There was an application loaded, but apparently, attempting to update the bootloader removed it – hence Application Version 0.00.

Thanks for the link – I had already tried what it suggested before posting, including disabling my virus-scanner and using DOS to copy the file – no results.

Thanks anyway!

Sean

0 Kudos
Reply