Problem regarding External RTC crystal

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem regarding External RTC crystal

Jump to solution
2,286 Views
Embionics
Contributor III

We have connected a 32Khz crystal(Abracon's ABS25-32.000KHZ-T) to be used as RTC clock input between PTC1 and PTE0. We have made such an arrangement in 40 different boards. Now we got a problem that crystal frequency is not coming. Might it be a problem with the crystal? Suggest me if there are any settings i need to do with the microcontroller when using crystal at PTC1

regards,

Embionics Technologies

Tags (3)
0 Kudos
Reply
1 Solution
1,955 Views
mjbcswitzerland
Specialist V

Hi

I am "guessing" you are using a KL25 (or similar).

If this is the case see Re: RTC_CLKIN and RTC_CLKOUT pins assignment on Kinetis and Re: KL25 RTC OSCILLATOR SELECTION

Unfortunately you can't use a crystal with this device since it doesn't have an oscillator - you would need to modify the boards and add a crystal oscillaor circuit in place fo the crystal (see the TWR-KL25Z48M circuit as reference.

Regards

Mark

View solution in original post

0 Kudos
Reply
1 Reply
1,956 Views
mjbcswitzerland
Specialist V

Hi

I am "guessing" you are using a KL25 (or similar).

If this is the case see Re: RTC_CLKIN and RTC_CLKOUT pins assignment on Kinetis and Re: KL25 RTC OSCILLATOR SELECTION

Unfortunately you can't use a crystal with this device since it doesn't have an oscillator - you would need to modify the boards and add a crystal oscillaor circuit in place fo the crystal (see the TWR-KL25Z48M circuit as reference.

Regards

Mark

0 Kudos
Reply