Problem programming srec on FRDM board, additional question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem programming srec on FRDM board, additional question

ソリューションへジャンプ
1,794件の閲覧回数
steve_fae
Senior Contributor I

Ok, followed Eric's suggestion on how to create a s19 file which turns out to be a *.hex file.  When I drop the file onto the MSD drive

nothing happens.  My application is trying to use the console function or printf out CDC to Tera Term.  It works in the normal manner when using the debugger

agent and such, but thought this would be a cool path for customers who need a special demo and don't want to mess with code compilation.  Is this beyond the scope of the MSD bootloader capabilities?

The file starts like this:

S0140000766973696F6E346C65676163792E68657837

S113000000300020FD060000F1080000FD0800009B

S1130010FD080000FD080000FD080000FD080000C8

.

.

.


ラベル(2)
0 件の賞賛
返信
1 解決策
1,671件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Can you try to use the DOS/cmd shell 'copy' command instead of using the Windows Explorer (press Windows+r, then enter the command 'cmd', then use the 'copy' command to copy the file to the bootloader).

I hope this helps.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,672件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Can you try to use the DOS/cmd shell 'copy' command instead of using the Windows Explorer (press Windows+r, then enter the command 'cmd', then use the 'copy' command to copy the file to the bootloader).

I hope this helps.

0 件の賞賛
返信