Problem programming srec on FRDM board, additional question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem programming srec on FRDM board, additional question

Jump to solution
1,801 Views
steve_fae
Senior Contributor I

Ok, followed Eric's suggestion on how to create a s19 file which turns out to be a *.hex file.  When I drop the file onto the MSD drive

nothing happens.  My application is trying to use the console function or printf out CDC to Tera Term.  It works in the normal manner when using the debugger

agent and such, but thought this would be a cool path for customers who need a special demo and don't want to mess with code compilation.  Is this beyond the scope of the MSD bootloader capabilities?

The file starts like this:

S0140000766973696F6E346C65676163792E68657837

S113000000300020FD060000F1080000FD0800009B

S1130010FD080000FD080000FD080000FD080000C8

.

.

.


0 Kudos
Reply
1 Solution
1,678 Views
BlackNight
NXP Employee
NXP Employee

Can you try to use the DOS/cmd shell 'copy' command instead of using the Windows Explorer (press Windows+r, then enter the command 'cmd', then use the 'copy' command to copy the file to the bootloader).

I hope this helps.

View solution in original post

0 Kudos
Reply
1 Reply
1,679 Views
BlackNight
NXP Employee
NXP Employee

Can you try to use the DOS/cmd shell 'copy' command instead of using the Windows Explorer (press Windows+r, then enter the command 'cmd', then use the 'copy' command to copy the file to the bootloader).

I hope this helps.

0 Kudos
Reply