Problem burning a binary file.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem burning a binary file.

5,849 Views
john71
Senior Contributor I

A bootloader program takes 17K. So my main program starts at address 0x5000.

In the linker file I configure

 

 

MEMORY {
  m_interrupts (RX) : ORIGIN = 0x00005000, LENGTH = 0x000001E8
  m_text      (RX) : ORIGIN = 0x00005410, LENGTH = 0x000FABF0
  m_data      (RW) : ORIGIN = 0x1FFF0000, LENGTH = 0x00010000
  m_data_20000000 (RW) : ORIGIN = 0x20000000, LENGTH = 0x00010000
  /*m_cfmprotrom  (RX) : ORIGIN = 0x00000400, LENGTH = 0x00000010*/
}

 

 

And generate a bin file (in KDS). When I open the file I see the main program starts at address 0x5000 in the file. So I cut out the block 0-0x4FFF and write the bin file starting at address 0x5000.

But when I exit the bootloader my main program doesn’t run.

I was trying to burn the file as is - the same result.

What is wrong?

 

In MCUXpresso bin file generated at address 0. What should I set in KDS?

0 Kudos
Reply
10 Replies

5,806 Views
john71
Senior Contributor I

I need to understand - if I generate a bin file and I see my program starts at 0x5000 in the file - should I start burning the file from this line?

Cause I burn from the offset but my program doesn't start. When I read back the data burned on the page - say at address 0x5000 - and compare with the bin file - I see the same data.

0 Kudos
Reply

5,797 Views
ErichStyger
Specialist I

I really cannot answer your questions, as they are too generic. It all depends on your device used, what bootloader you use, how you have architected your application.

Just looking at the address or the bin file or the memory does not say much: you have to understand what your bootloader does and what your application does. Best for this is if you step with the debugger through your bootloader and check what it is doing: then you will know what and why it is failing.

0 Kudos
Reply

5,793 Views
john71
Senior Contributor I

First I erase all pages

case FC_STATE_EREASE:
{
    m_pRecFrame[m_uiRecCount++] = uiReadData;
    if( m_uiRecCount >= sizeof(uint32_t) )
    {
        // check the address validity
        if ( (m_RecFrame.uiAddress < RELOCATION_VERTOR_ADDR) || (m_RecFrame.uiAddress > (USER_FLASH_END_ADDR-ERASE_BLOCK_SIZE)) ) 
        {
            UART_Send(FC_CMD_NACK);
        }
        else
        {
            if(!Flash_EraseSector(m_RecFrame.uiAddress))
            {
                erase_count++;
                UART_Send(FC_CMD_ACK);
            }
            else	
                UART_Send(FC_CMD_NACK);			
        }

	g_ucFC_State = FC_STATE_WORKING;
    }
}
break;

And I see erase_count equals the pages I need to erase (bin_file_size / page_size) + 1.

Next I write all pages by write chunks (64 bytes)

case FC_STATE_WRITE_DATA:  
{
    m_pRecFrame[m_uiRecCount++] = uiReadData;
    if( m_uiRecCount > (m_RecFrame.Length + sizeof(uint32_t) ))
    {
        Memcpy_Byte((uint8_t *)&m_ucDataBuff[0], (uint8_t *)&m_RecFrame.DataBuff[0], m_RecFrame.Length);
        uiNumberCount ++;

        // check address is valid
            if ( (m_RecFrame.uiAddress < RELOCATION_VERTOR_ADDR) || (m_RecFrame.uiAddress > (USER_FLASH_END_ADDR-ERASE_BLOCK_SIZE)) )
            {
                UART_Send(FC_CMD_NACK);
            }
            else
            {
               if( !Flash_Write(m_RecFrame.uiAddress, (uint8_t *)&m_ucDataBuff[0], m_RecFrame.Length) )
               {
                   write_count++;
                   UART_Send(FC_CMD_ACK);
              }
              else
                  UART_Send(FC_CMD_NACK);
          }
          g_ucFC_State = FC_STATE_WORKING;
    }
}
break;

And I see write_count equals number of chunks I sent.

So I pretty sure the burn process was successful. The same (official) bootloader burns srec file and the main program runs. So it seems like something wrong with the  bin file.

0 Kudos
Reply

5,764 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @john71,

The code that you attached is from your bootloader? If this is the case, how are you jumping to the application after loading the binary? Did you change the PSP, MSP and VTOR before jumping?

Best Regards,

Alexis Andalon

0 Kudos
Reply

5,757 Views
john71
Senior Contributor I

I can jump to a user application by pressing the Quit button.

 

case FC_CMD_QUIT:
{
    SCB_VTOR = RELOCATION_VERTOR_ADDR;
    JumpToUserApplication(RELOCATION_VERTOR_ADDR);
}
break;

 

Or I can release the boot  pin on power up

 

if ((cMAINT_GetVal()) && (cBOOT_GetVal()))
{
    for(;;)
    {
       if( !FC_Communication() )
       {
           if( g_ucFC_State == FC_STATE_NULL)
           {
               uiNullCounter++;
               if(uiNullCounter > 0xFFFF)
               {
                    uiNullCounter = 0;
                    uiRepeatCount++;
                    UART_SendChar(0xFC);
                }
            }
        }
    }
}
else
{
    #ifdef FLASH_LOCATION
    SCB_VTOR = RELOCATION_VERTOR_ADDR;
    JumpToUserApplication(RELOCATION_VERTOR_ADDR);
    #endif
}

 

The code is the same that works with in Universal Bootloader (AN2295).

I created a bin file from a srec file (srec_cat.exe MK10.srec -o MK10.bin -binary). and I see the first line

00000000  FF FF FF FF FF FF FF FF FF FF FF FF 76 FF FF FF 

then goes a zeros block and the code starts at offset

00005000  00 00 00 20 A9 FB 01 00 79 23 02 00 79 23 02 00   and so on.

Now I start to burn the srec file with the Universal Bootloader and set a break point at the first write to a flash.

And I see the burn data starts with FF FF FF FF FF FF FF FF FF FF FF FF 76 FF FF FF not with 00 00 00 20 A9 FB 01 00 79 23 02 00 79 23 02 00. Is there something I miss to understand?

 

0 Kudos
Reply

5,745 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @john71,

The application note mention that the address to the new vector table is 0x4000, make sure that all the macros point to the new application address.

Also, if I'm understanding correctly, the first block is discarded but the first line of the discarded block is being written in the first position?

Best Regards,

Alexis Andalon

0 Kudos
Reply

5,734 Views
john71
Senior Contributor I

So what the binary file offset I should start to burn at address 0x4000 in the flash? If I understand correct at the address 0x4000 in the flash I should start to burn the line that starts at 0x4000 in the binary file?

0 Kudos
Reply

5,671 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @john71,

The address should match the RELOCATION_VERTOR_ADDR mentioned in your bootloader, also, could you let me know which MCU are you using?

Best Regards,

Alexis Andalon

0 Kudos
Reply

5,663 Views
john71
Senior Contributor I

MCU is  MK10FN1M0VLQ12.

Tags (1)
0 Kudos
Reply

5,654 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @john71,

For recent MCUs in the Kinetis family there's support for a bootloader, but unfortunately for this MCU the MCUBoot is not supported but you could take a look at the reference material for this.

Best Regards,

Alexis Andalon

0 Kudos
Reply