Probable mistake in K60 reference manual?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Probable mistake in K60 reference manual?

Jump to solution
2,261 Views
kaitav
Contributor III

Hi,

I was going through the USBDCD module description of K60 microcontroller reference manual and observed that on "Page 1453 of the K60P144M150SF3RM pdf, section 49.3.1 USB signal descriptions, Table 49-5" there is a typo in the second column against "dvdd" signal. Shouldn't this be 3.3V digital supply instead of 1.2V?

Thanks,

Kaitav

0 Kudos
Reply
1 Solution
2,044 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi Kaitav

The dvdd to the USB DCD is an internal signal. The main VDD is internally regulated down to 1.2V to power the digital logic in the chip including the digital supply for the USB DCD.

Have a great day,
Vicente

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
2,045 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi Kaitav

The dvdd to the USB DCD is an internal signal. The main VDD is internally regulated down to 1.2V to power the digital logic in the chip including the digital supply for the USB DCD.

Have a great day,
Vicente

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,044 Views
kaitav
Contributor III

Hi Vicente,

Thanks for enlightening me with this.

Have a great weekend,

Kaitav

0 Kudos
Reply