Probable mistake in K60 reference manual?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Probable mistake in K60 reference manual?

跳至解决方案
1,384 次查看
kaitav
Contributor III

Hi,

I was going through the USBDCD module description of K60 microcontroller reference manual and observed that on "Page 1453 of the K60P144M150SF3RM pdf, section 49.3.1 USB signal descriptions, Table 49-5" there is a typo in the second column against "dvdd" signal. Shouldn't this be 3.3V digital supply instead of 1.2V?

Thanks,

Kaitav

0 项奖励
回复
1 解答
1,167 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Hi Kaitav

The dvdd to the USB DCD is an internal signal. The main VDD is internally regulated down to 1.2V to power the digital logic in the chip including the digital supply for the USB DCD.

Have a great day,
Vicente

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,168 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Hi Kaitav

The dvdd to the USB DCD is an internal signal. The main VDD is internally regulated down to 1.2V to power the digital logic in the chip including the digital supply for the USB DCD.

Have a great day,
Vicente

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,167 次查看
kaitav
Contributor III

Hi Vicente,

Thanks for enlightening me with this.

Have a great weekend,

Kaitav

0 项奖励
回复