Probable mistake in K60 reference manual?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Probable mistake in K60 reference manual?

ソリューションへジャンプ
2,276件の閲覧回数
kaitav
Contributor III

Hi,

I was going through the USBDCD module description of K60 microcontroller reference manual and observed that on "Page 1453 of the K60P144M150SF3RM pdf, section 49.3.1 USB signal descriptions, Table 49-5" there is a typo in the second column against "dvdd" signal. Shouldn't this be 3.3V digital supply instead of 1.2V?

Thanks,

Kaitav

ラベル(3)
0 件の賞賛
返信
1 解決策
2,059件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Hi Kaitav

The dvdd to the USB DCD is an internal signal. The main VDD is internally regulated down to 1.2V to power the digital logic in the chip including the digital supply for the USB DCD.

Have a great day,
Vicente

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,060件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Hi Kaitav

The dvdd to the USB DCD is an internal signal. The main VDD is internally regulated down to 1.2V to power the digital logic in the chip including the digital supply for the USB DCD.

Have a great day,
Vicente

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,059件の閲覧回数
kaitav
Contributor III

Hi Vicente,

Thanks for enlightening me with this.

Have a great weekend,

Kaitav

0 件の賞賛
返信