Preipheral Drivers for Freescale Freedom KL25Z FRDM Platform

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Preipheral Drivers for Freescale Freedom KL25Z FRDM Platform

ソリューションへジャンプ
5,582件の閲覧回数
gurindersinghgi
Contributor III

I am in a search for peripheral drivers for Freescale freedom FRDM Kl25Z Platform , i am creating a project in CW without using Processor Expert , can anyone help with that , as CW builds the project with just MKL25Z128 hedder support , there is no driver or peripheral library available .

ラベル(2)
0 件の賞賛
返信
1 解決策
2,990件の閲覧回数
adriansc
Contributor IV

Hi,

In the attach File you can find folders an .c files for FRDM-KL25.

1. Create a new Bareboard Project for KL25

2. Copy the Folders into the project (Check paths.txt to see where to drop each folder).

3. Add the paths for the Compiler and Preproccesor

(Right click on the Project name->Properties->C/C++ Build->Settings->ARM Ltd Windows GCC C Compiler->Directories) and also in ARM Ltd Windows GCC C Compiler->Directories.

Let me know if you have any problem.

Hope this helps.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,991件の閲覧回数
adriansc
Contributor IV

Hi,

In the attach File you can find folders an .c files for FRDM-KL25.

1. Create a new Bareboard Project for KL25

2. Copy the Folders into the project (Check paths.txt to see where to drop each folder).

3. Add the paths for the Compiler and Preproccesor

(Right click on the Project name->Properties->C/C++ Build->Settings->ARM Ltd Windows GCC C Compiler->Directories) and also in ARM Ltd Windows GCC C Compiler->Directories.

Let me know if you have any problem.

Hope this helps.

0 件の賞賛
返信
2,990件の閲覧回数
gurindersinghgi
Contributor III

Thanks for great help, I guess a recent update to sample code package [SC V4] has been posted on Freescale website, which has some sample Code warrior bearboard projects , thanks for the help ,

1 question : can i directly add other peripherals such as I2C, Etc from SC package to the project ,

what all modifications has to be made to the package ?

0 件の賞賛
返信
2,990件の閲覧回数
adriansc
Contributor IV

Hi,

That is right there is an update for Sample Code Package. This update has support for CW projects, you can find there the platinum project which handles a variety of modules for KL25Z. Most of the examples that you can find in recent update are only compiled for IAR but we are working to migrate them to CW :smileywink:.

There is a drivers folder: ....\KL25\kl25_sc\klxx-sc-baremetal\src\drivers. This contain peripherals code, such as initialization, functions and more for some modules. You can add this to your project, the only thing that you will need to do is to add the paths of the files in project´s properties.

Probably when you compile your project, you will find some issues with register´s masks, because some masks has not the same name in the different IDEs. You will be able to fix them easy because names are very similar.

Hope this helps.

Regards.

0 件の賞賛
返信