Precision of MMA8451

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Precision of MMA8451

2,892 Views
michelmeunier
Contributor I

Hello,

I am very surprised by the very bad precision of the MMA8451 on the FRDM-KL25Z.

When the board is fixed, the (x,y,z) values of the 1g is changing quite a lot from one read to an other. For example the z value change between 3931 to  3968. It's about 1%. Why have 14bits precision, when the true precision is not good? I am in 2g mode to have the best precision.

Michel

0 Kudos
Reply
5 Replies

2,697 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Michel,

For the best noise performance, it is recommended to select the lowest possible ODR and use both Low Noise (LNOISE bit = 1) and High Resolution (MODS [1:0] = 0b10) modes. For more information please refer to our AN4075.

Hope it helps.

Regards,

Tomas

0 Kudos
Reply

2,697 Views
michelmeunier
Contributor I

Hello

I have tried the Tomas' explainations:

  error=MMA1_Disable();

  error=MMA1_ReadReg8(XYZ_DATA_CFG,&valeur);

  valeur&=0xFC; //2g mode

  error=MMA1_WriteReg8(XYZ_DATA_CFG,valeur);

  error=MMA1_ReadReg8(CTRL_REG1,&valeur);

  valeur|=0x3C; //1.56Hz rate plus low noise

  error=MMA1_WriteReg8(CTRL_REG1,valeur);

  error=MMA1_ReadReg8(CTRL_REG2,&valeur);

  valeur&=0xF7;

  valeur|=0x10; //High resolution mode

  error=MMA1_WriteReg8(CTRL_REG1,valeur);

  error=MMA1_ReadReg8(F_SETUP,&valeur);

  valeur&=0xFC; //no FIFO

  error=MMA1_WriteReg8(F_SETUP,valeur);

  error=MMA1_Enable();

And it's only a little bit better:

my board is on a table and the z value is between 4026 and 4080! And, no I am not a the top of a buiding during an earthquake ;-)

I thing I am going to take an other system because the MMA8451 is really to bad and it hasn't enough precision for my goal.

Michel

0 Kudos
Reply

2,697 Views
bobpaddock
Senior Contributor III

USB is not always the cleanest of power supplies. Take a look at the VTI/Now Murta SC3100 .  It can sense me typing from several feet away (at first I thought the part was junk and noisy tell I figured out the typing connection). http://www.murata.com/en-sg/products/sensor/accel/sca3100 Analog Devices makes parts in the aircraft grade with lots of zeros in the price tag if noise is that big of issue. Consider using a Median Filter:  http://embeddedgurus.com/stack-overflow/tag/median-filter/

0 Kudos
Reply

2,697 Views
bobpaddock
Senior Contributor III

How clean is the power supply?

0 Kudos
Reply

2,697 Views
michelmeunier
Contributor I

It is powered by the FRDM-KL25 board. And The board is powered by USB of my computer.

0 Kudos
Reply