Power sequencing scheme of MK70FN1M0VMJ12

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Power sequencing scheme of MK70FN1M0VMJ12

1,607 Views
puspamnayak
Contributor III

Hi,

Want to know is there any power sequencing scheme for turning on MK70FN1M0VMJ12 with DDR2, USB, RS485, NAND Flash and other peripherals on board.

Request you to reply at earliest

Thanks and regards,

Puspam Nayak

Tags (1)
0 Kudos
Reply
2 Replies

1,483 Views
daweiyou
NXP Employee
NXP Employee

Hi:

From Datasheet of K70:

VDD_INT is Core supply voltage, same power source with VDD

5.5 Power sequencing

Voltage supplies must be sequenced in the proper order to avoid damaging internal

diodes. There is no limit on how long after one supply powers up before the next supply

must power up. Note that VDD and VDD_INT can use the same power source.

The power-up sequence is:

1. VDD

2. VDD_INT

3. VDDA

4. VDD_DDR

The power-down sequence is the reverse:

1. VDD_DDR

2. VDDA

3. VDD_INT

4. VDD

Dawei You(尤大为)

0 Kudos
Reply

1,482 Views
puspamnayak
Contributor III

Hi,

Many thanks for the reply. I found the same in datasheet yesterday

Best Regards,

Puspam N

0 Kudos
Reply