Power consumption in sleep mode with reference oscillator enabled on KW41

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Power consumption in sleep mode with reference oscillator enabled on KW41

949件の閲覧回数
ppd
Contributor II

Hi,

On my KW41Z512M4 based board, in VLPS (bypass mode), I measure a power consumption of ~10 uA with the reference oscillator (OSC 32 MHz) disabled (which is OK, that's what I'm aiming for) and ~4 mA :smileyalert: when the oscillator is enabled (that is, enabled prior to entering sleep mode). 

What causes the huge current consumption in the second scenario? Isn't the OSC disabled in VLPS? Or maybe it's a XCVR issue I am overlooking?

Thanks,

Paul.

ラベル(1)
0 件の賞賛
返信
1 返信

809件の閲覧回数
gerardo_rodriguez
NXP Employee
NXP Employee

Hello Paul,

Could you let me know with what demo application are you making this test and exactly how are you enabling/disabling the reference oscillator? The reference oscillator can be enabled by a Radio link layer, an internal SoC clock mode, by an external pin request or by the RF_OSC_EN bits from the RSIM CONTROL register. The Figure 3-20 from the reference manual illustrates this. 

pastedImage_1.png

The reference oscillator can also work in VLPS. So, the extra current measured will depend on what modules are using this clock.

Regards,

Gerardo

0 件の賞賛
返信