Power Distribution of K66F

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Power Distribution of K66F

5,152 次查看
haozh
Contributor I

Power distribution of K66F

Hello Team, 

I have a question regarding the power distribution of K66F schematics. If I power the board through the openSDA usb connector, the P3V3_SDA is powered through U17 which means J18 should shorted by R61. However, I find that both R84 and R61 is not populated on the board. Can you tell me where the power of P3V3_SDA is from if J18 is not connected. Also, I found that SDA_VOUT33 is not connected too.

Regards,

Hao

0 项奖励
回复
3 回复数

5,089 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Hao,

P3V3_SDA is powered through J7(SDA_VOUT33).

P5V_SDA SDA_VOUT33.png

SDA_VOUT33 P3V3_SDA.png

About the VREGIN and VOUT33, here you can refer:

USB regulator bus supply.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

5,089 次查看
haozh
Contributor I

Thank you very much Robin. It is very helpful. Does any NXP mcu has the USB regulator embedded?

Hao

0 项奖励
回复

5,089 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

All the Kinetis MCU with USB module has the USB regulator embedded.

0 项奖励
回复