Possible errata on KL25 Reference Manual

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Possible errata on KL25 Reference Manual

ソリューションへジャンプ
4,844件の閲覧回数
danielcolon
Contributor II

Hello".

I've been trying to configure the PIT Module changing the registers manually following the KL25 Reference Manual (KL25P80M48SF0) it didn't work, so I look at the code in Kinetis SDK and I realize the bits numbers on the Reference Manual tables were backwards. I mean, the bit 0 appears as bit 31 on the Reference Manual.

After configuring the registers with bits as they should be, the PIT module works fine.

Is the Reference Manual wrong? or I missed some note that indicates this backwards convention?

Note: I don't sure if this question goes here.

ラベル(2)
0 件の賞賛
返信
1 解決策
4,676件の閲覧回数
mjbcswitzerland
Specialist V

Hi

All of the PIT registers in the KL25 user manual are numbered incorrectly.
They should count 31...0 rather than 0...31.

As far as I am aware this error is limited to the PIT section of only that manual - all other manuals seem to have it correct.

Regards

Mark

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
4,676件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Sorry for the inconvenience. I have report this issue to our document team.

Best Regards,

Robin

0 件の賞賛
返信
4,677件の閲覧回数
mjbcswitzerland
Specialist V

Hi

All of the PIT registers in the KL25 user manual are numbered incorrectly.
They should count 31...0 rather than 0...31.

As far as I am aware this error is limited to the PIT section of only that manual - all other manuals seem to have it correct.

Regards

Mark

0 件の賞賛
返信
4,676件の閲覧回数
danielcolon
Contributor II

Thank You!

Wich other manuals do you know about the KL25Z?

Regards.

Daniel.

0 件の賞賛
返信
4,676件の閲覧回数
mjbcswitzerland
Specialist V

Daniel

I meant all other manuals to other parts (eg. KL26, KL27 etc.).

Regards

Mark

0 件の賞賛
返信