Possible BUG in USB 5.0 Stack (yes, another one)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Possible BUG in USB 5.0 Stack (yes, another one)

Jump to solution
2,229 Views
johnstrohm
Contributor III

In file usb_dev.c, lines 276-278, I find the following:

            if((event->direction == USB_RECV) && (event->buffer_ptr != NULL))

                OS_dcache_invalidate_mlines((void*)event->buffer_ptr,event->len);

            service_ptr->service(event,service_ptr->arg);

In file adapter_bm.h, line 64, I find the following:

#define OS_dcache_invalidate_mlines(p,n)

The combination of these lines looks, to me, suspiciously like one of those old-time cartoon bombs, with the big,black sphere, and the fuse sizzling away.  The hapless customer who attempts to use the library on bare metal, without MQX, is likely to find himself chasing an interesting problem.  Once the preprocessor does its thing, the compiler will see:

            if((event->direction == USB_RECV) && (event->buffer_ptr != NULL))

                service_ptr->service(event,service_ptr->arg);  /* indentation added to emphasize issue */


which is probably not exactly what is wanted, if the direction happened to be USB_SEND.

May I respectfully suggest the following modification?

            if((event->direction == USB_RECV) && (event->buffer_ptr != NULL))

            {

                OS_dcache_invalidate_mlines((void*)event->buffer_ptr,event->len);

            }

            service_ptr->service(event,service_ptr->arg);

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
2,068 Views
makeshi
NXP Employee
NXP Employee

Firstly thanks for your raising the problem and help us improve the USB’s stack’s quality.  Since there is a “;” , the combination of  these line by compiler will be to:

if((event->direction == USB_RECV) && (event->buffer_ptr != NULL))

;

service_ptr->service(event,service_ptr->arg); 

So it will not impact the functionality of code. But I appreciate your code that you suggest change to. Such code is more clear and unambiguous. We accept it and change it in our stack.

View solution in original post

0 Kudos
Reply
2 Replies
2,069 Views
makeshi
NXP Employee
NXP Employee

Firstly thanks for your raising the problem and help us improve the USB’s stack’s quality.  Since there is a “;” , the combination of  these line by compiler will be to:

if((event->direction == USB_RECV) && (event->buffer_ptr != NULL))

;

service_ptr->service(event,service_ptr->arg); 

So it will not impact the functionality of code. But I appreciate your code that you suggest change to. Such code is more clear and unambiguous. We accept it and change it in our stack.

0 Kudos
Reply
2,068 Views
johnstrohm
Contributor III

Thank you very much for the clarification.

I missed the semicolon.  You're right, the semicolon makes it safe.  It still bothers me.

Thank you for accepting the change suggestion.

0 Kudos
Reply