Porting Kinetis_twrmk21n512_msd_host demo program to K22 MCU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Porting Kinetis_twrmk21n512_msd_host demo program to K22 MCU

655 Views
rhana
Contributor III

What are the steps required to port this demo to the K22 (MK22FN1M0)?

0 Kudos
Reply
1 Reply

521 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Customer need to compare the hardware platform for K21 and K22, if both using the same frequency external crystal/oscillator. For both chips with the same USB module, the USB related code should be same. The porting focus on hardware platform difference.

And I find there is USB stack for K22, which also include USB HOST MSD demo.

Please check below link for more detailed info:

Freescale bare metal (no OS) USB Stack Rev. 5

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MEDICALUSB&fpsp=1&tab=Design_Tools_Ta...


Wish it helps.
best regards
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply