Porting KBOOT

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Porting KBOOT

2,406件の閲覧回数
jorgehoraciogon
Contributor II

Hello everyone! I need to port the kinetis bootloader to the MK53DN512CMD10 uC, the document "Kinetis Bootloader v2.0.0 Reference Manual" that I´m using indicate to me I need a header from the webpage of NXP, but actually that header does not appear. Somebody could tell me if that file exist? (MK53DN512CMD10.h)

I would be very thankful for your answer.

0 件の賞賛
返信
1 返信

2,336件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,

The MK53DN512CMD10.h is the previous kind of head version, please choose the MK53DZ10.h which support the K50_100 series MCU.

Hope it helps.


Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信