Please help me recommend a brushless DC motor development kit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Please help me recommend a brushless DC motor development kit

1,338件の閲覧回数
simithli
Contributor I

Please help me recommend a brushless DC motor development kit, that is, including the controller, procedures and motors.
Specific requirements:
1, the controller chip needs to be KEA128 or 64, if not, others are OK,but its performance and programming is closer to the KEA128;
2, the program needs to be for BLDC with position hall sensors;
3, the program needs to achieve forward, reverse, speed regulation , other basic functions and some commonly used algorithms;
4, driven motor and power circuit can be changed, the latter need to test the motor of different power levels;
Thank you very much.

タグ(1)
0 件の賞賛
返信
1 返信

1,189件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Simith,

Pls refer to the website for KEA family application to control BLDC.

3-phase Sensorless BLDC Motor Control RD|NXP 

If you use Hall sensor to detect position of rotor, as you know that the KEA has three FTM modules, FTM0 can be used to generate 3 pair PWM signals, FTM1 and FTM2 can be used to detect Hall signal with capture function so that rising/falling edges of three hall signals can be used to trigger interrupt, compute the speed. You can connect 3 hall signals to FTM1 or FTM2  channels for example FTM1_CHx, it is okay. For forward, reverse, speed regulation, it is dependent on software.

I think any KEA family is okay to control BLDC.

Hope it can help you

BR

Xiangjun Rong

0 件の賞賛
返信