Pins for FTM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Pins for FTM

4,105 Views
Andrei13
Contributor III

I am using frdm ke16z. Can you provide a pinout diagram and a user manual for the board, not for the uC. TY!

 

Tags (1)
0 Kudos
Reply
5 Replies

4,034 Views
CarlosGarabito
NXP TechSupport
NXP TechSupport

If you check the electrical diagram, on page 3, there is the PTB0 pin connector to the UART0_RX_TGTMCU, following the connection to page 4, it says that it connects to the UART0_RX_TGTMCU_BUF and this to the UART0_TX_TGTMCU_R of the OPENSDA MK20DX128VFM5. You will not find it on the arduino connector.

 

0 Kudos
Reply

4,029 Views
Andrei13
Contributor III

But for LPUART1_RX it s on PTC6. PTC6 it s on arduino's jumper J1, on pin 2. Right? TY!

0 Kudos
Reply

4,013 Views
CarlosGarabito
NXP TechSupport
NXP TechSupport

@Andrei13Yes, that's right

0 Kudos
Reply

4,055 Views
Andrei13
Contributor III

But for example i need to connect a receiver on the UART RX pin. This is PTB0 and i can t find it on the arduino J. TY! @CarlosGarabito 

0 Kudos
Reply