Pin voltage

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Pin voltage

1,465 次查看
al_silantyev
Contributor I

I work with the mk60dn512vlq10 microcontroller and my problem is that I don’t understand how to configure the GPIO pin. For pin, the fact is that a 3.3V pulse arrives on the pin, but the microcontroller "sees" this pulse only with an offset voltage of 1.1V or lower, but I need that with a 3.3V voltage and an offset voltage of 1.65V, the pin sees a pulse and my interrupt handler works

0 项奖励
回复
1 回复

1,389 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi aleksandr,

Sorry i may not understand your question. Can you draw a signal waveform diagram to illustrate the function you want to achieve?
You can find the electrical characteristics in "Table 1. Voltage and current operating requirements" of K60P144M100SF2V2.

Voltage and current operating requirements.png

Do you consider use the comparator module? You can setup the defined compare voltage.

CMP.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复