Peripheral Chip Select on K22

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Peripheral Chip Select on K22

1,430件の閲覧回数
gibson486
Contributor I

How are the Peripheral Chip Select pins different than just taking a normal digital out and using that as a chip select?

0 件の賞賛
返信
2 返答(返信)

1,317件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Andrew Chin,

     Do you mean you want to use the GPIO in K22  as the peripheral chip select pins? Or the module's pin in the K22, if it is the module's pin, which module you are using?

     If you just use the GPIO, you need  check the IO current driver ability, whether it is enough to driver your peripheral chip, more details, please refer to the K22 datasheet.

    Wish it helps you!

If you still have question, please contact me!

Have a great day,

Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,317件の閲覧回数
mjbcswitzerland
Specialist V

Hi

The K22 has two different SPI interfaces, one with 1 deep FIFO and 1 with 4 byte deep FIFO.

When using the 4 deep FIFO it is possible to program the behaviour of the CS for each byte prepared - in case of the single depth FIFO this is not an option so the advantage is not the same on all SPI instances - one needs to be careful since the driver of each may need to be different!

When using CS peripheral lines it is also possible to specifiy some timing behavior so that there is a certain delay before or after data.

In most cases it is however just as easy (and sometimes easier) to control them with a port output instead.

Regards

Mark

0 件の賞賛
返信