Performance analysis and measurement using code warrior 10.4?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Performance analysis and measurement using code warrior 10.4?

ソリューションへジャンプ
1,712件の閲覧回数
anand-k
Contributor III

Hello,

I want to do advanced performance measurement analysis using code warrior.

I am using code warrior(eclipse based) v10.4 IDE and our controllers is KL25.

Could anyone help me/suggest out with this?

Thanks in advance,

Anand K

ラベル(2)
0 件の賞賛
返信
1 解決策
1,413件の閲覧回数
BlackNight
NXP Employee
NXP Employee

The KL25 features an on-chip trace buffer (MTB).

First Steps with the P&E Tracelink | MCU on Eclipse

Debugging ARM Cortex-M0+ Hard Fault with MTB Trace | MCU on Eclipse

Based on that trace, the program flow can be analyzed, and the 'SA' part in CodeWarrior can provide performance analysis.

If you are using FreeRTOS, there is FreeRTOS+Trace which gives you performance information:

Tracing with FreeRTOS+Trace from Percepio | MCU on Eclipse

I hope this helps.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,414件の閲覧回数
BlackNight
NXP Employee
NXP Employee

The KL25 features an on-chip trace buffer (MTB).

First Steps with the P&E Tracelink | MCU on Eclipse

Debugging ARM Cortex-M0+ Hard Fault with MTB Trace | MCU on Eclipse

Based on that trace, the program flow can be analyzed, and the 'SA' part in CodeWarrior can provide performance analysis.

If you are using FreeRTOS, there is FreeRTOS+Trace which gives you performance information:

Tracing with FreeRTOS+Trace from Percepio | MCU on Eclipse

I hope this helps.

0 件の賞賛
返信