Peg Lite Download?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Peg Lite Download?

2,258件の閲覧回数
dvona
Contributor II

Where is the PEG Lite Free download for Kinetis?  If I start here: http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=PEGLT&fpsp=1

I see a download button, but following it through there is no place that actually takes me to a download for PEG Lite?  It turns out to be circular bringing back to the original place.  What am I missing?

Regards,

-Dan

ラベル(1)
タグ(3)
0 件の賞賛
返信
2 返答(返信)

2,025件の閲覧回数
CJarvis
NXP Employee
NXP Employee

A PEG Lite license can be obtained by going to http://www.nxp.com/peglite and select the link in the overview description to "obtain a free PEG Lite license".  The option is also available from the "Buy" tab on the same page.

0 件の賞賛
返信

2,025件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hi Dan,

You can to send an email to [email protected] to request a license key and download link.

Best Regards,

Luis

0 件の賞賛
返信