Hi,
I'm have a couple of questions about the PGA on the MK20DX256VLH7.
1. PGA Chop Feature
According to the Reference Manual section 31.3.18 ADC PGA Register (ADCx_PGA) the chip doesn't have the PGAOFSM and PGACHPb fields.
There is a section 6.6.1.4 16-bit ADC with PGA characteristics with Chop enabled in the Data Sheet.
Is this feature only available in some versions of this chip?
2. Use of external reference with VrefOut
The data sheet and reference manual indicate that it is possible to use an external reference applied to VrefOut with the internal reference disabled. It is unclear to me what voltage restrictions apply to this external reference. For example, is it possible to extend the PGA input compliance range by use of an external 3.0V reference?