PDBx and Vector Table K24

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PDBx and Vector Table K24

ソリューションへジャンプ
2,373件の閲覧回数
DaveTonyCook
Contributor IV

Hi,

The K24 has 2 PDB's but I can only find 1 exception vector in the vector table. PDB0_IRQHandler... where is PDB1_IRQHandler As I understand it the vector table come predefined.  Please help Thanks

ラベル(1)
タグ(1)
1 解決策
2,210件の閲覧回数
mjbcswitzerland
Specialist V

Hi

The K24 has only one PDB, but this has 2 channels. Therefore there is only one interrupt vector.

I don't believe that any parts have more that one PCB.

Regards

Mark

µTasker Kinetis support

PDB based application in chapter 2 of http://www.utasker.com/docs/uTasker/uTaskerADC.pdf

元の投稿で解決策を見る

3 返答(返信)
2,211件の閲覧回数
mjbcswitzerland
Specialist V

Hi

The K24 has only one PDB, but this has 2 channels. Therefore there is only one interrupt vector.

I don't believe that any parts have more that one PCB.

Regards

Mark

µTasker Kinetis support

PDB based application in chapter 2 of http://www.utasker.com/docs/uTasker/uTaskerADC.pdf

2,210件の閲覧回数
DaveTonyCook
Contributor IV

Hi Mark,

After enabling the interrupt PDBIE = 1 and setting the interrupt delay IDLY = 1 then 1000 I cant see any difference in the frequency of the interrupt... any clues?

Thanks

2,210件の閲覧回数
DaveTonyCook
Contributor IV

Whoops sorry for wasting your time.  The interrupt delay is relative to the trigger input to the PDB