PCA9698 I2C setting

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCA9698 I2C setting

1,407 Views
hfabbasi
Contributor III

I am new to I2C protocol and trying to turn LED on/off connected to bank 0, pin 0 in MCUXpresso software by NXP. Would there be any code whihc I can use as reference for I2C or atleast guide me how to configure PCA9698 for turning LED on/off ? What would be the sequence of device (slave) address, output configuration register and command register for output?

0 Kudos
Reply
1 Reply

1,389 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello

Hope you are well.
Which device are you using to interface the PCA9698?
You can refer to the SDK examples if they are available in the device you are using. You can find the commands and the sequence required at the datasheet of the PCA9698: https://www.nxp.com/docs/en/data-sheet/PCA9698.pdf

Let me know if this is helpful, if you have more questions do not hesitate to ask me.
Best regards,
Omar

0 Kudos
Reply