P.E. K70 and LCD Question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P.E. K70 and LCD Question

ソリューションへジャンプ
2,301件の閲覧回数
crezyoz
Contributor IV

I am just getting started with PE. Trying to build an LCD driver for a monochrome Electro Luminiescent display. (HYSNC/VSYNC/ 2 wire interface/1bpp)

 

However, when I go to set the Pixel Clock there is no entry in the Component Inspector.  It is blank. Everything else went ok.

 

Any advice?

 

 

0 件の賞賛
返信
1 解決策
2,150件の閲覧回数
crezyoz
Contributor IV

Found it.. sorry for the noise.

 

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,151件の閲覧回数
crezyoz
Contributor IV

Found it.. sorry for the noise.

 

0 件の賞賛
返信
2,150件の閲覧回数
squadmcu
NXP Employee
NXP Employee

Hi Phil! How did you solve this?

0 件の賞賛
返信
2,150件の閲覧回数
crezyoz
Contributor IV

After a good deal of trial and error I determined that the type of EL display I am using can not be driven from the K70 in the 1bpp mode. Apparently the K70 can not keep the pixel clock running continuously in that mode only . So I had to use 8bpp mode and only use one bit to drive the display. This had a negative impact on my design because it meant I had to add DDR to the design. The frame buffers grew to 128k and I need 4 of them. I REALLY wish it had worked. I hope they make it very clear in the next set of docs for the LCD interface. It was an expensive week figuring that one out.

0 件の賞賛
返信