Overvoltage protection for TWR-KM34Z50M ADC inputs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Overvoltage protection for TWR-KM34Z50M ADC inputs

1,974 Views
svenmoeller
Contributor II

Hello,

is there already an overvoltage protection included for the ADC inputs?

Or what would be the best way of implementing a protection? (the voltage may not exceed +-250mV)

Simply using two antiparallel diodes? -> Are there existing diodes with a forward bias of 250mV?

Thank you

0 Kudos
Reply
2 Replies

1,723 Views
perlam_i_au
Senior Contributor I

Just as you mention antiparallel diodes could be a good protection I would also suggest a simple RC filter in order to avoid noise.


Have a nice day,
Perla Moncada

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,723 Views
Wlodek_D_
Senior Contributor II

Hello,

Thank you for your post, however please consider moving it to the right community place (e.g. Kinetis Microcontrollers ) to get it visible for active members.

For details please see general advice Where to post a Discussion? (https://community.freescale.com/docs/DOC-99909 )

Thank you for using Freescale Community.

0 Kudos
Reply