Over voltage Power Supply effects on Kinetis K26 microcontroller IO's states

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Over voltage Power Supply effects on Kinetis K26 microcontroller IO's states

1,216件の閲覧回数
puneeth_bheemar
Contributor I

Hello,

we are using Kinetis K26 microcontroller in our design. based on the datasheet, supply voltage is 3.3V +/- 10%. in normal operation supply voltage is well with in the mentioned range of 3.3V+/-10%.

However we would like to know the IO's state when power supply range goes above the maximum voltage of 3.6V (maximum of 4.1V).

will controller retain the previous state of IO's?

will the state of IO's will be tri-state / High impedance?

Thanks,

Puneeth KB

ラベル(2)
0 件の賞賛
返信
1 返信

1,154件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi Puneeth,

No, it won't. Although supply power over 3.6v may harm to the device, it will not change the pin into tri-state or high-impedance.

Regards,

Jing

0 件の賞賛
返信