Optimal clock settings for external resonator

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Optimal clock settings for external resonator

1,940件の閲覧回数
zainali
Contributor II

Hi,

I trying to find the optimal settings for system oscillator. I am using external clock source with 8Mhz resonator. The oscillator configuration in reference manual shows 3 modes,

zainali_0-1637328036745.pngzainali_0-1637328036745.png

Can anyone guide what configuration should i choose as 8 Mhz is overlapped. Also is gain linked to the accuracy?

The Microcontroller i am using is MK10DN512 and schematic of oscillator can be seen below.

zainali_1-1637328756166.pngzainali_1-1637328756166.png

 

Thanks

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,933件の閲覧回数
bobpaddock
Senior Contributor IV

High Gain Mode 2 would be the most reliable.

Gain is more linked to power consumption and start time than accuracy.
Accuracy is determined mostly by the grade of the resonator.

I can't speak to this particular chip, however I've seen reliability problems over the years with using low power (low gain) oscillators.  They don't always start reliably across voltages and temperature ranges.

If your resonator has internal caps, disable any built-in caps that the chip may offer.

0 件の賞賛
返信

1,925件の閲覧回数
zainali
Contributor II

@bobpaddock  thanks for valuable information.


For sake of knowledge, is there any reason to go with high gain mode 2.

Thanks again

 

0 件の賞賛
返信