Opensda .s19 file for FRDM- K82F

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Opensda .s19 file for FRDM- K82F

1,257 Views
sanket_joshi
Contributor I

hi,

I am working on FRDM-K8F board. It has open SDA support.  It is not entering bootloader mode if if i press the reset button and then power up. So i request you to share with me .s19 or srec file for opensda as I am using PE Micro as debuger.

Labels (1)
0 Kudos
Reply
1 Reply

1,177 Views
miduo
NXP Employee
NXP Employee

Hello,

The OpenSDA can been download from here: OpenSDA Serial and Debug Adapter|NXP 

However I highly recommend you may have a look at this post, especially when you can not see the "BOOTLOADER"

https://community.nxp.com/message/1098505

0 Kudos
Reply