OpenSDA Flasher works, but Debugger does not work

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OpenSDA Flasher works, but Debugger does not work

ソリューションへジャンプ
10,014件の閲覧回数
quevedo
Contributor V

I have a Freescale FRDM board, with a KL25 target processor and OpenSDA interface. In the beginning it was working fine, but now the DEBUG-APP_Pemicro_v102.SDA app is not working, although the MSD-FRDM-KL25Z_Pemicro_v107.SDA works OK.

What I mean is, I can load the flasher (MSD) app to load a SREC file, and the board will accept it (the program will load and start running). However, if I load the debugger (DEBUG) app and try to debug a project (I tried that with a project that was previously working fine), I get an error window (file OpenSDAError.jpg attached), and then when I click OK I get a window asking me to select the connection I want to use. If I retry connection, I get another error (file OpenSDAError2.jpg attached). I am using CodeWarrior 10.3 Beta.

When I plug the board with the debugger app previously loaded, I can see the CDC and debugger devices in my hardware manager (windows XP 32-bits), and the bootloader mode accepts the app files. I tried to reinstall the drivers, but I don't know what can be going wrong.

Any ideas?

ラベル(2)
0 件の賞賛
返信
1 解決策
9,293件の閲覧回数
quevedo
Contributor V

I was already using 10.3 before the problem occurred, in both computers. I just reinstalled it in the computer where the problem appeared, and now it is working OK.

元の投稿で解決策を見る

0 件の賞賛
返信
9 返答(返信)
9,293件の閲覧回数
quevedo
Contributor V

Now I am using CW10.4, and OpenSDA is working fine with the board that I had to replace the KL25 from!

0 件の賞賛
返信
9,293件の閲覧回数
FarhanH
Contributor III

I have run into the same problem with the K20 freedom board (after the first debug, all subsequent debugger connections fail). There has to be a way to fix this without re-installing CW 10.3. I have the latest version with all the updates.

0 件の賞賛
返信
9,293件の閲覧回数
FarhanH
Contributor III

Ok, I have a partial workaround for this. If I leave the debug connection as USB Multilink and terminate/remove my debug sessions, I should be ok. I just have to select OpenSDA every time the P&E connection manager window pops up (this gets annoying). If I select OpenSDA as the connection under the debugger options or create a new OpenSDA option, it stops working permanently.

0 件の賞賛
返信
9,293件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hello,

If you cannot connect, that P&E connection manager shows up, and here you can choose your new connection.

But this new connection is only temporary: if you debug again, it tries to connect to the previous connection.

To change it permanently, go into the debug/run configuration and change it to the new (permanent) settings.

See http://mcuoneclipse.com/2013/04/15/a-new-freedom-board-frdm-k20d50m-with-arm-cortex-m4/

for how to change the connection.

Pay attention that you select 'SWD' (Single Wire Debug): I occasionally have missed it, and then the connection does not work. I believe this is what you are seeing.

I hope this helps.

0 件の賞賛
返信
9,293件の閲覧回数
FarhanH
Contributor III

Thanks! The SWD checkbox seems to be the key.

0 件の賞賛
返信
9,293件の閲覧回数
apanecatl
Senior Contributor II

Hi Antonio, the first error screenshot leads me to believe you might have selected the wrong package while you were creating your project, please make sure you are selecting the MKL25Z128 variant as shown in the image.

2852_2852.png

9,293件の閲覧回数
quevedo
Contributor V

That was the first thing I had checked. Target was correct. Also, other projects that were previously loading presented the same errors.

I tried the same projects in my home computer, and they loaded without any problems. Thus, I supposed that CW installation in my office computer got corrupted somehow.

I reinstalled my CW10.3 Beta in my office computer, and the problem did not occur anymore.

0 件の賞賛
返信
9,293件の閲覧回数
apanecatl
Senior Contributor II

Well KL microcontrolles will only work with CW10.3, the KL variants are not included in CW 10.2

9,294件の閲覧回数
quevedo
Contributor V

I was already using 10.3 before the problem occurred, in both computers. I just reinstalled it in the computer where the problem appeared, and now it is working OK.

0 件の賞賛
返信