OpenSDA / DAPLink do not update - stuck in MAINTENANCE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OpenSDA / DAPLink do not update - stuck in MAINTENANCE

4,116件の閲覧回数
Anonymous
適用対象外

This looks like an old problem and the solution is available from mbed but following it I still cannot upgrade firmware.

My FRDM-K64F board debug firmware was corrupted and I followed the instructions on https://os.mbed.com/blog/entry/DAPLink-bootloader-update/   to the letter . I got OpenSDA to boot as MAINTENANCE but on the step #5 the upgrade to the DAPLink did not work: after the upgrade firmware still boots as MAINTENANCE. As a result, it is only a storage device but not recognized as a debug probe. Tried to upload OpenSDA binary from OpenSDA Serial and Debug Adapter|NXP 

the same result - the board stuck in MAINTENANCE and no debug probe recognized.

Please help.

ラベル(1)
3 返答(返信)

2,919件の閲覧回数
Bing
Contributor II

I solved the same problem by erasing MK64 flash with an external JLINK.

In my case some buggy codes put MK64 resetting constantly, which in turn hold the onboard OpenSDA on MAINTENANCE mode via reset pin.

Hope you can revive your board by the same approach.

0 件の賞賛
返信

3,571件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Please check the version of the DAPLink bootloader or interface firmware in the DETAILS.TXT when the device is mounted as MAINTENANCE or DAPLINK.

version of the DAPLink bootloader.png
I am using the DAPLink rev0244 OpenSDA v2.2 Bootloader(0244_k20dx_bl_0x5000.bin) and DAPLink rev0244 firmware application(k20dx_frdmk64f_if_crc_legacy_0x5000.bin) download from OpenSDA Serial and Debug Adapter|NXP.

DAPLink rev0244.png

After firmware application is installed, you should be able to find it in Device Manager.

Device Manager.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,571件の閲覧回数
Anonymous
適用対象外

I did all that sequence on two PCs (WIndows 7 and Win 10) - the same result - still MAINTENANCE mount as as external drive but no probe recognized.

0 件の賞賛
返信