OpenOCD problem withFRDM-K64F

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OpenOCD problem withFRDM-K64F

3,582件の閲覧回数
pratiekbhadrana
Contributor III

Hello,

I tried upgrading the mbed firmware in my FRDM-K64F board to start debugging using OpenOCD, but it still does not work. Here is a screenshot of the errors that I get in console

I have also used the -f kinetis.cfg as mentioned in some other thread. I am now shifting to the Segger interface. But I would like to know if there is some way to use OpenOCD.

ラベル(2)
0 件の賞賛
返信
7 返答(返信)

3,271件の閲覧回数
pratiekbhadrana
Contributor III

The Segger interface is working!! But is there any solution to use OpenOCD?

0 件の賞賛
返信

3,271件の閲覧回数
pratiekbhadrana
Contributor III

pastedImage_0.jpg

0 件の賞賛
返信

3,271件の閲覧回数
mjbcswitzerland
Specialist V

Hi

OpenOCD looks to need the CMSIS-DAP debugger installed - I don't know whether this works with KDS since usually the P&E one tends to be used.

Rowley Crossworks does use CMSIS-DAP for debugging and, when working with this IDE, I load the attached debugger instead. (Again not necessarily the latest version but has been used successfully).

Regards

Mark

Kinetis: µTasker Kinetis support

K64: µTasker Kinetis FRDM-K64F support / µTasker Kinetis TWR-K64F120M support

For the complete "out-of-the-box" Kinetis experience and faster time to market


3,271件の閲覧回数
pratiekbhadrana
Contributor III

Thank you Mark. I will try this and inform you about the results. Thanks for your help:smileyhappy:

0 件の賞賛
返信

3,271件の閲覧回数
mjbcswitzerland
Specialist V

Hi

The mbed boot loader doesn't allow debugging with KDS.

You need to use the P&E loader instead (which then doesn't support USB-MSD drag.and-drop loading).

I have attached a version that I have used for some time - there may be newer ones available on the P&E web size.

Regards

Mark

Kinetis: µTasker Kinetis support

K64: µTasker Kinetis FRDM-K64F support / µTasker Kinetis TWR-K64F120M support

For the complete "out-of-the-box" Kinetis experience and faster time to market

0 件の賞賛
返信

3,271件の閲覧回数
pratiekbhadrana
Contributor III

Hello Mark, the Segger interface is working. If you check in mcuoneclipse, Erich Styger's blog he has mentioned that to use OpenOCD on the OpenSDA v2 interface, it is necessary to upgrade the firmware to version 211. I am interested in using OpenOCD basically because it allows me to flash and debug other custom boards as well.

0 件の賞賛
返信

3,271件の閲覧回数
pratiekbhadrana
Contributor III

Ok I will try out Segger first and if it does not work then I will try your option.

0 件の賞賛
返信