On Board Programming MKV31F256VLH12 with external Watchdog Fails

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

On Board Programming MKV31F256VLH12 with external Watchdog Fails

ソリューションへジャンプ
2,667件の閲覧回数
hamsdybamsdy
Contributor I

We use the MKV31F256VLH12 controller from NXP in a new design.

Programming takes place via the SWD interface.

Programmer: J-Link Plus from Segger.

Also an external watchdog with an open drain output is provided

in the circuit.

The watchdog output is separted over a 470R Resistor from the Reset Pin of the

controller.

The watchdog currently forces a reset approx. Every 400ms.

Unfortunately  also during the programming cycle.

 Is there a possibility that the programmer (J-Link Plus) keeps the RESET signal permanently high while the controller is being programmed?

A jumper between the output of the watchdog and the reset pin of the controller is not an option (lost / forgotten).

 

best regards

Helmut

0 件の賞賛
返信
1 解決策
2,624件の閲覧回数
hamsdybamsdy
Contributor I

Hello,

Meanwhile I have a solution. The Segger Programmer doesn`t need a connection to the Reset Pin
during the programming cycle. In the textfixture for programming and test we connect the reset pin of the Controller with Vdd during the programming cycle. Then the watchdog has no chance to reset
the controller.

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,648件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

After some consideration, I wasn’t able to come up with a viable option to do this given the limitations.

Perhaps the Segger support team could have a better insight on how to achieve this.

 

Regards,

Edwin.

0 件の賞賛
返信
2,625件の閲覧回数
hamsdybamsdy
Contributor I

Hello,

Meanwhile I have a solution. The Segger Programmer doesn`t need a connection to the Reset Pin
during the programming cycle. In the textfixture for programming and test we connect the reset pin of the Controller with Vdd during the programming cycle. Then the watchdog has no chance to reset
the controller.

 

 

0 件の賞賛
返信