Oled SSD1306 Library

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Oled SSD1306 Library

9,932件の閲覧回数
javierhernande1
Contributor IV

Hello,

Exist some library to control the SSD1306 via I2C with the FRDM-K64F?

BR

ラベル(1)
8 返答(返信)

9,103件の閲覧回数
LeonardoP4
Contributor I
0 件の賞賛
返信

9,465件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Javier,

   Do you still have any question about this topic?

   If you still have question about it, please kindly let me know.


Have a great day,
Kerry

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

9,465件の閲覧回数
javierhernande1
Contributor IV

Hello,

Thank you, I have left this for a few weeks. 

Best regards

0 件の賞賛
返信

9,465件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Javier,

   If you still have question about this case, please update it.

   If your question is solved, please help to mark the correct answer, just to close this case, thank you!


Have a great day,
Kerry

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

9,465件の閲覧回数
MarcoGiammarini
Contributor III

9,465件の閲覧回数
BlackNight
NXP Employee
NXP Employee

There is a Processor Expert component (McuOnEclipse Components: 26-Dec-2017 Release | MCU on Eclipse ) which supports both SSD1306 and SH1106.

If not using Processor Expert, the plain C files are here: McuOnEclipseLibrary/McuSSD1306.c at master · ErichStyger/McuOnEclipseLibrary · GitHub 

A project for FRDM-K64F is available here: mcuoneclipse/Examples/KDS/FRDM-K64F120M/FRDM-K64F_SSD1306 at master · ErichStyger/mcuoneclipse · Git... 

I hope this helps,

Erich

9,465件の閲覧回数
javierhernande1
Contributor IV

Thank you, I have seen the project in github but it's for PE.

BR

0 件の賞賛
返信