Obvious bug in 5.0 USB stack, in file usb_cdc.c

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Obvious bug in 5.0 USB stack, in file usb_cdc.c

Jump to solution
1,755 Views
johnstrohm
Contributor III

Routines USB_Cdc_Allocate_Handle() and USB_Cdc_Free_Handle both walk through cdc_device_array.

cdc_device_struct_t   cdc_device_array[MAX_CDC_DEVICE];

static usb_status USB_Cdc_Allocate_Handle(cdc_handle_t* handle)

{

    uint32_t cnt = 0;

    for (;cnt< MAX_CDC_DEVICE;cnt++)

    {

        if (cdc_device_array[cnt].controller_handle == NULL)

        {

            *handle = (cdc_handle_t)&cdc_device_array[cnt];

            return USB_OK;

        }

    }

    return USBERR_DEVICE_BUSY;

}

static usb_status USB_Cdc_Free_Handle(cdc_handle_t handle)

{

    int32_t cnt = 0;

    for (;cnt< USBCFG_DEV_MAX_CLASS_OBJECT;cnt++)

    {

        if (((cdc_handle_t)&cdc_device_array[cnt]) == handle)

        {

            OS_Mem_zero((void *)handle, sizeof(cdc_device_struct_t));

            return USB_OK;

        }

    }

    return USBERR_INVALID_PARAM;

}

If some poor maintenance guy changes USBCFG_DEV_MAX_CLASS_OBJECT, and forgets to update MAX_CDC_DEVICE, he will break USB_Cdc_Free_Handle().

The for-statement in USB_Cdc_Free_Handle()

    for (;cnt< USBCFG_DEV_MAX_CLASS_OBJECT;cnt++)

should be identical to the for-statement in USB_Cdc_Allocate_Handle().

    for (;cnt< MAX_CDC_DEVICE;cnt++)

Labels (2)
Tags (3)
1 Solution
1,554 Views
jeremyzhou
NXP Employee
NXP Employee

Hi John,

I'll report this issue to AE team for checking and thank you very much for your focus on Freescale product.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,555 Views
jeremyzhou
NXP Employee
NXP Employee

Hi John,

I'll report this issue to AE team for checking and thank you very much for your focus on Freescale product.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply