OTA update KW24D

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OTA update KW24D

1,387 Views
edalmanzar
Contributor I

I'm trying to update my KW24D in the program NXP test tool 12 through OTA MAC and there is very little information about it. Someone could explain me the steps to made the ota update. 

I have changed the code, I have also tried another program with ota. But the KW24D remains unanswered to the ota update

#ota update

Tags (1)
0 Kudos
Reply
1 Reply

1,228 Views
stephanie_m
NXP TechSupport
NXP TechSupport

Hello, 

Could you please check the chapter 5. Over-the-air Programming of the IEEE 802.15.4 MAC Demo Applications User's Guide? 

This guide provides information about the 802.15.4 MAC Over-the-Air Programmer (MAC OTA Programmer) based on the Freescale 802.15.4 Media Access Controller (MAC) implementation.

The file it's located in the Connectivity Software of the KW24 under the path 

C:\<installation path>\MKW2xD_ConnSw_1.0.2\docs\wireless\IEEE 802.15.4

Regards, 

Estephania 

0 Kudos
Reply