OPENSDAv2 for KEA128

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OPENSDAv2 for KEA128

1,515 Views
daweiyou
NXP Employee
NXP Employee

Hi:

I check the DAP source code, which doesn't include example for TRK-KEA128, pls help check where I could find the resource? thx.

Labels (1)
0 Kudos
Reply
2 Replies

1,388 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Dawei,

     DO you mean the DAP source code is the oepnsdav2 MBED source code?

    That code is for the K20 chip, and used as the debugger, just like the FRDM on board debugger with MK20DX128VFM5, when you use the opensda v2.0, and change the firmware to JLINK, then the Jlink firmware will support the KEA128 chip.

Wish it helps you!

If you still have question, please let me know!

Have a great day,
Kerry

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,388 Views
daweiyou
NXP Employee
NXP Employee

got, thx Kerry.

Yes, I found source code for DAP, but it don't support KEA till now.

 The original debugger on TRK-KEA128 is from PE micro.

I want to implement simple flasher using DAP source code.

0 Kudos
Reply