Number of 16 bit timers and 32 bit timers in MK26FN2M0VLQ18

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Number of 16 bit timers and 32 bit timers in MK26FN2M0VLQ18

819 次查看
prasannanaik
Contributor III

Hi,

   I want to know the exact number of 16 bit timer channels and 32 bit timer channels in MK26FN2M0VLQ18 as i couldn't find this information in datasheet as well as reference manual. Also, the number of capture inputs available in this part.

Thanks and best regards,

Prasanna

标签 (1)
0 项奖励
回复
1 回复

767 次查看
miduo
NXP Employee
NXP Employee

Hello,

Timers
• Four Periodic interrupt timers  (32 bit)
• 16-bit low-power timer (16 bit)
• Two 16-bit low-power timer PWM modules  (16 bit)
• Two 8-channel motor control/general purpose/PWM timers (16 bit)
• Two 2-ch quad decoder/general purpose timers  (16 bit)
• Real-time clock (32 bit)

pastedImage_1.png

0 项奖励
回复