Hi
I'm using TWR-K70120M in which I was working on the ETHERNET part. So in the MQX RTOS 4.1.0 folder (C:\Freescale\Freescale_MQX_4_1\rtcs\examples\eth_to_serial) i found the "eth_to_serial" example. Before compiling i read the readme.pdf then after i made the required changes in the user_config.h file as follows,
#define BSPCFG_ENABLE_ITTYF 1
#define BSP_DEFAULT_IO_CHANNEL_DEFINED
#define BSP_DEFAULT_IO_CHANNEL "ittyf:"
After all this, i compiled the MQX libraries and then flashed the code. Now the problem is, according to the readme.pdf file i supposed to get the following message on the uart,
Application listening on following ip addresses:
IPv4 Address: 192.168.1.202, port:23
IPv6 Address 0: fe80::200:5eff:fea8:1ca, port: 23
Waiting for incoming connection...
which is i'm not getting but on the TCP terminal i saw the following message,
Ethernet <-> Serial bridge
So now I'm confused what should be the reason for not establishing "Serial <-> Ethernet bridge" connection. Any help will be really appreciated!!
Regards
Omkar Dixit
Solved! Go to Solution.
Hi
The issue is solved now. Actually initially i have enabled only the one macro which is "#define BSPCFG_ENABLE_ITTYF 1" and then when i enabled "#define BSPCFG_ENABLE_ITTYC 1" it got worked!
Regards
Omkar
 
					
				
		
 danielchen
		
			danielchen
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi @omkardixit
Please check the network configurations:
From readme file:
3) Connect the evaluation board and your PC to same Ethernet network.
Did you connect the evaluation board to your PC with a cable and configured it correctly?
Regards
Daniel
Hi
The issue is solved now. Actually initially i have enabled only the one macro which is "#define BSPCFG_ENABLE_ITTYF 1" and then when i enabled "#define BSPCFG_ENABLE_ITTYC 1" it got worked!
Regards
Omkar