Non-Volatile Data storage in MK60DN512VMD10

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Non-Volatile Data storage in MK60DN512VMD10

跳至解决方案
1,477 次查看
nbjasani
Contributor III

Hi,

   Is there any Non-Volatile Data storage memory in MK60DN512VMD10 Device? Is it possible to store data in Flash memory? i mean Flash memory not FlexNVM/FlexRAM. Is this device having FlexRAM?

Thanks

Nandish Jasani.

1 解答
1,407 次查看
mjbcswitzerland
Specialist V

Hi

The K60DN512VDM100 has some OTP (one-time-programmable) memory and also any Flash that is not used for code can be used to store data into.

https://www.utasker.com/docs/uTasker/uTaskerFileSystem_3.PDF - OTP, parameter and file system code for this chip is available on GITHUB in the open source uTasker project for the K60, including flash operation simulation.

Regards

Mark
[uTasker project developer for Kinetis and i.MX RT]

在原帖中查看解决方案

2 回复数
1,408 次查看
mjbcswitzerland
Specialist V

Hi

The K60DN512VDM100 has some OTP (one-time-programmable) memory and also any Flash that is not used for code can be used to store data into.

https://www.utasker.com/docs/uTasker/uTaskerFileSystem_3.PDF - OTP, parameter and file system code for this chip is available on GITHUB in the open source uTasker project for the K60, including flash operation simulation.

Regards

Mark
[uTasker project developer for Kinetis and i.MX RT]

1,407 次查看
nbjasani
Contributor III

Hi,

   Thanks for your reply, i will go with flash for data storage, i have found some code example in MCUXpresso for flash data storage.

Thanks and Regards,

Nandish Jasani.

0 项奖励
回复