No documentation for HVP-KV58F

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

No documentation for HVP-KV58F

1,945件の閲覧回数
kenbarfield
Contributor I

Hi,

I have HVP-KV58F modules in hand.

I can’t find any documentation to go with it. No board details. No code. 

Can some kind NXP person set some expectations for this?

Thx,

Ken

タグ(2)
0 件の賞賛
返信
3 返答(返信)

1,837件の閲覧回数
hieutran
Contributor I

Hi Xiangjun, I have the same board HVP-KV58F. However my bootloader is corrupt since I accidentally press the Reset button. I can not find the binary bootloader file of this kit on NXP site. Could someone upload it? Thanks!

Robert

0 件の賞賛
返信

1,837件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Pls download the bootloader from the link:

Kinetis Bootloader|NXP 

Maybe you have to modify the code based on KV5x feature.

BR

Xiangjun Rong

0 件の賞賛
返信

1,837件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Ken,

Pls refer to the link for the high voltage power stage board and the corresponding daughter card.

High-Voltage Development Platform|NXP 

BR

Xiangjun Rong

0 件の賞賛
返信